Browse FAQs

What is the part number of the R38 resistor on the ATV66C23N41 ATV66C28N41 ATV66C31N41 primary side of the transformer?

Published date: 24 June 2020

Issue:
ATV66C23N41 / ATV66C28N41 / ATV66C31N41 R38 resistor part number on primary side of the transformer

Product Line:
ATV66 

Environment:
R38
 
Cause:
 n/a

Resolution:
This is a 5 ohms 40w resistor .The part number is 2619997465.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.