undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What does ``low differential `` mean regarding a 9007C62A2 or C68T5 ?<br /><br />
Differential is the distance between the point where the contacts change state on actuation and the point where the contacts move back to their ``at rest ``position . A low differential type has a 2 degrees vs. a 4 degrees ( for the standard switches ) distance or spread .



CTA-ID : 2021229

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.