Browse FAQs

Are the Class 8810 Type S two speed starters available in a NEMA 3R enclosure?

Published date: 29 June 2020

Issue:
Identifying Two-Speed starters enclosure options

Product Line: 
8810 Two-Speed Starters

Environment:
NEMA Contactors and Starters

Resolution:
Two speed starters are only available in NEMA 1, 4, 4X, 7 & 9 or 12.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.