Browse FAQs

What is the part number of the key on a Keyed Selector Switch operator ZB5AG03D?

Published date: 21 June 2020

Issue:
Key for keyed selector switch operator ZB5A***D Part number.

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony XB5

Resolution:
The device uses 8D1 key, and should be ordered using cat. no. ZBD8D1, which will provide two keys.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.