Browse FAQs

What is the mechanical and electrical operating cycles of the 9422 Type T disconnect switches?

Published date: 21 June 2020

Issue:
 Life expectancy of the 9422 Type T disconnect switches

Product Line: 
Operating Mechanism & Disconnect Switches

Environment:
9422T Disconnect Switch

Resolution:
Per UL 98 these switches must provide the following minimum operations based on amperage size:

30 Amp, 6 cycles per minute maximum, 6000 cycles with current, 4000 cycles without current.
60 Amp, 6 cycles per minute maximum, 6000 cycles with current, 4000 cycles without current.
200 Amp, 5 cycles per minute maximum, 6000 cycles with current, 2000 cycles without current.
400 Amp, 4 cycles per minute maximum, 1000 cycles with current, 5000 cycles without current.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.