Browse FAQs

For the XVP indicating banks, which terminal goes to which unit in the stack?

Published date: 21 June 2020

Issue:
XVP wiring installation

Product Line:
Tower Lights and Beacons

Environment:
50mm Diameter Harmony® XVP

Resolution:
The terminals are numbered 1 through 5 to correspond to the units in succession up the stack.  So the first unit is #1, second unit is #2. 
See the attached instructions, page 14.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.