Issue:
Operating mechanism for Tesys U Starters
Product Line:
IEC Contactors and Starters
Environment:
TeSys U Starters
Resolution:
Use the LU9AP00 (shaft & mounting bracket kit *) PLUS either the LU9AP11 (Black/Blue handle) or the LU9AP12 (Red/Yellow handle). The handle kits are rated NEMA 1/12 and can be used with the LUB or LU2B self-protected starter bases only. There is no through-the-door operator for the LUS and LU2S starter bases.
* the square connector end is included with the handle not the LU9AP00
Operating mechanism for Tesys U Starters
Product Line:
IEC Contactors and Starters
Environment:
TeSys U Starters
Resolution:
Use the LU9AP00 (shaft & mounting bracket kit *) PLUS either the LU9AP11 (Black/Blue handle) or the LU9AP12 (Red/Yellow handle). The handle kits are rated NEMA 1/12 and can be used with the LUB or LU2B self-protected starter bases only. There is no through-the-door operator for the LUS and LU2S starter bases.
* the square connector end is included with the handle not the LU9AP00
Released for:Schneider Electric USA