Browse FAQs

Does Square D offer an alternate lug for a single 750kcmil wire for the EZM1400FS?

Published date: 10 June 2020

Issue:
Product Design Features 

Product Line:
EZM Metering Equipment

Environment:
Terminal Lug Data

Cause:
Alternate wire sizes

Resolution:
For the LH molded case switch used in this main device, use the AL400LH7 lug kit. The lug kit includes only 1 lug and accepts (1) #350-750kcmil Al/Cu wire. For the Main Neutral use the NEMA pad kit catalog number MMSK2 with an ILSCO lug, part number TA8002N(not sold by Square D).

For additional alternate lugs for the EZM1400FS see the below attached CAD drawing. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.