Browse FAQs

Are Softstarters acceptable for use in a Fire Pump applications?

Published date: 15 June 2020

Issue:
Softstarters for use in a Fire Pump applications

Product line:
Altistart 22 48 ATS22 ATS48

Environment:
all

Cause:
Fire pump systems typically require the motors to run until they fail, without faulting the controller

Resolution:
No. The softstarters are not rated for Fire pump requirements and does not meet the requirements.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.