Browse FAQs

Why does RDY flash on the ATV31?

Published date: 19 June 2020

Issue:   
RDY flash on the ATV31
 
Product Line:   
ATV31
 
Environment:  
All serial numbers
 
Cause:  
Customer said drive was flashing RDY.
 
Resolution:   
Flashing display normally indicated current limit mode. However, if this is occurring in the ready mode, it is likely due to incorrect motor parameter settings.
Specifically, it could be that the COS (motor power factor) is set to 1.
OR
Check the +10 and +24 VDC power supplies. It could be that they are being pulled down.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.