Browse FAQs

What is the difference between 9007C62B1 AND 9007C62B2 ?

Published date: 21 June 2020

Issue:
 How does 9007C62B1 differ from 9007C62B2 ?

Product Line: 
Limit Switches and Sensors

Environment:
Nema Limit Switches

Resolution:
Both are exactly the same physical parts. 9007C62B1 is set up at the factory for CCW operation only, whereas the 9007C62B2 can be actuated CW and CCW. The switch can be converted in the field from B1 to B2, or from B2 to B1. Instructions are given for this operation in the sensor catalog, 9006CT0101, page 477.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.