Browse FAQs

How many knockouts are there for the cable glands on a XALK and XALD?

Published date: 21 June 2020

Issue:
Knockouts on the XALK and XALD control stations 

Product Line:
Harmony Control Stations and Enclosures

Environment:
XAL 22mm Control Stations

Resolution:
There are 2 knock-outs PG 13.5 cable glands, maximum capacity 0.47 in (12 mm). One on the top and one on the bottom.  There is also a knock-out at the back for cable entry, maximum capacity 0.55 in (14 mm).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.