Browse FAQs

What is the function of the LUA8E20 and how many contacts does it have?

Published date: 21 June 2020

Issue:
What is the use of the LUA8E20 and how many contacts does it include?

Product Line: 
Contactors and Starters IEC

Environment:
Tesys U combination motor starters

Resolution:
This is a control circuit contact block consisting of (2) normally open contacts used only with the LUB__ and LU2B__ U-Line combination motor controllers. The contact is used to disconnect the control source voltage when the U-Line handle operator is in the OFF position. This contact block meets the requirement of NEC 430-74.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.