Browse FAQs

How can input phase loss fault be disabled with the Altivar 58 drive?

Published date: 19 June 2020

Issue:
Altivar 58 input phase loss fault disable.

Product Line:
Altivar 58

Environment:
All

Cause:
N/A

Resolution:
Go to menu 6 (FLt - fault menu)
Set the IPL  parameter (Input Phase Loss) to no.
This will allow the drive to continue running without PHF fault if there is a loss of input phase voltage. This does not disable other faults in the drive.
See keypad programming manual for additional details.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.