Browse FAQs

What are the auxiliary contacts for the Powerpact H, J, L, M, P and R frame breakers?

Published date: 12 March 2019

Issue:  
Looking for the proper aux switch part number for Powerpact H, J, L, M, P and R breakers.  

Product Line:
Electrical Distribution Equipment

Environment:
Circuit Breakers
PowerPact H, J, L, M, P and R

Resolution:
Standard:
1A/1B       S29450
2A/2B       S29450 x 2
3A/3B       S29450 x 3 (only L, M, P and R frames)

Low level gold flash:
1A/1B      S29452
2A/2B      S29452 x 2
3A/3B      S29452 x 3 (only L, M, P and R frames)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.