Browse FAQs

Why is the 9421V1W30 rated 4/4X ``indoor only`` and not Nema 3R or outdoor rated?

Published date: 25 June 2020

Issue:
Is the 9421V1W30 NEMA 3R rated?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Vario Metallic Enclosed Switches

Resolution:
Because the KCF1PZ handle is rated IP65, Nema 1 and Nema 12 only. These handles are not stabilized against the effects of ultraviolet light.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.