Browse FAQs

How do the preset speeds operate when using 8 presets with the Altivar 58 drive?

Published date: 20 June 2020

Issue:
Configure preset speeds using 8 presets with the Altivar 58 drive.

Product Line:
ATV58 Drives

Environment:
All 

Cause:
Preset speeds

Resolution:
See attached keypad programming manual for additional details.

For 8 preset speeds, three inputs are used. One logic input must be programmed for PS2 (2 preset speeds). The second input is set to PS4 (4 preset speeds). A third input is set to PS8 (8 preset speeds)
In the chart below, the input set for PS2 is shown as LIX. The PS4 input is LIY. The PS8 input is LIZ.
The chart shows a 1 for active inputs and a 0 for inputs that do not have 24 VDC applied. The combination of the three inputs determines the speed that the drive will run.
High speed (HSP), Low speed (LSP) and Preset speed 2 (PS2) through preset speed 7 (PS7) can be set in the SET adjustment menu 2.

LIz    LIy     LIx          Frequency Reference
0       0       0    =    LSP ( low speed ) + AI reference
0       0       1    =    SP2 ( preset speed 2 )
0       1       0    =    SP3 ( preset speed 3 )
0       1       1    =    SP4 ( preset speed 4 )
1       0       0    =    SP5 ( preset speed 5 )
1       0       1    =    SP6 ( preset speed 6 )
1       1       0    =    SP7 ( preset speed 7 )
1       1       1    =    HSP ( high speed )


CTA-ID : 2015916

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.