Browse FAQs

Can the S33595 test set be used to test the LXL type MicroLogic breaker?

Published date: 11 July 2018

Issue:
Is the S33595 test set compatible wth the LXL type Micrologic breaker?

Product Line:
Circuit Breaker

Environment:
Micrologic Breaker

Resolution:
No. The S33595 is a test set for newer versions of MicroLogic breakers. The UTS3 test set is used to test the LXL breaker.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.