Browse FAQs

What is the decibel level for the XB5KS* annunciators?

Published date: 21 June 2020

Issue:
What is the sound measurement level for the XB5KS* annunciators?

Product Line: 
Push Button and Operator Interface

Environment:
22 mm Push Button

Resolution:
The current XB5KS* are rated for 85 decibels at 1 meter. Before 2005 they were rated 80 decibels at 1 meter.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.