Browse FAQs

What is the difference between the LUB32 and the new LUS32 starter base?

Published date: 24 June 2020

Issue:
Difference between the LUB32 and the new LUS32 starter base

Product Line: 
Contactor and Starter - IEC

Environment:
TeSys U Combination Motor Starter

Resolution:
The LUS32 is starter base approved for group motor installations with upstream short circuit protection. The LUB32 is self-protected starter base which is approved for group motor installations or UL508 Type E self-protected combination motor controller.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.