Browse FAQs

How is the XACA pendant going to be affected by the obsolescence of the XA2 and XB2 lines ?

Published date: 21 May 2020

Issue:
Needs to know how does the XACA pendant going to be affected by the obsolescence of the XA2 and XB2 lines.

Product Line: 
Push Buttons and Operator Interface

Environment:
22mm Push buttons

Resolution:
There are 69 old ZA2B/ZB2B parts that will still be available in addition to the XACA9411 through 19 booted push button operators and XENG**** & XACS**** contact blocks . The legend plates associated with the XACA pendants will also remain available.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.