Browse FAQs

Are the ZB4 and ZB5 double headed push buttons interlocked?

Published date: 21 May 2020

Issue:
Need to know if the double headed push button are interlocked.

Product Line: 
Push Buttons and Operator Interface

Environment:
XB4/XB5 Harmony Push Buttons

Resolution:
Double headed push button are not interlocked with each other. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.