Browse FAQs

Are optional lugs available for the EZM3400TB and EZM3400TBCU Series M03 Main devices?

Published date: 10 June 2020

Issue:
Alternate Lugs

Product Line:
EZM Metering Equipment

Environment:
Alternate wire sizes needed

Cause:
Application

Resolution:
Yes, optional lugs are available for use in the EZM3400TB and EZM3400TBCU Series M03 Tap Boxes. Refer to the attached CAD Drawing #3368, for the list of Lugs that have been evaluated for use in these devices.
NOTE: Alternate Lugs in these devices will require the use of Lug Landing Pad, catalog number EZMSK2 (order separately).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.