Browse FAQs

What is the part number for the replacement nut that fixes the XB6 type operator to the panel?

Published date: 21 May 2020

Issue:
Which nut is used to fix the XB6 type operator to the panel?

Product Line: 
Push Buttons and Operator Interface

Environment:
Harmony 16 mm XB6/ZB6 Plastic Push Buttons

Resolution:  
Use the ZB6Y002 part number.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.