Browse FAQs

What is the part number of the shaft mounting bracket for 9421LS8, LS10, LS12 and LS13 ?

Published date: 21 May 2020

Issue:
Is the shaft mounting bracket for 9421LS8, LS10, LS12 and LS13 replaceable?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9421 Type L Circuit Breaker Mechanism

Cause:
Product selection

Resolution:
The shaft mounting or support bracket is included with the shaft and is not supplied separately. Must order the appropriate complete shaft kit 9421LS8, LS10, LS12 or LS13.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.