Browse FAQs

What is the maximum current rating for the 8501KP/KPD relay?

Published date: 01 June 2020

Issue: 
Maximum current rating for the 8501KP/KPD relay

Product Line: 
Relays and Timers

Environment:
Square D 8501 Type K Relays

Resolution:
The new F series is 12 amps continuous per pole up to 240 volts AC. All other series are 10 amps continous per pole up to 240 volts AC. On the 3 pole version it is a maximum of 20 amps total (sum of all 3 poles).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.