Browse FAQs

What lugs can be used on the EZM32000CBU main device?

Published date: 10 June 2020

Issue:
Current design features

Product Line:
EZM Metering Equipment

Environment:
Main Phase and Neutral Lugs

Cause:
installation and application

Resolution:
Various lugs are available for field installation on this device. Refer to the drawing for available lugs: EZM32000CBU Drawing

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.