Browse FAQs

Is there a difference between Class 2510 Type KO2 and Type KO6?

Published date: 22 June 2020

Issue:
What is the difference between 2510KO2 and 2510KO6?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
2510 type K switches

Answer:
The 2510KO6 has higher HP ratings at 460V and 600V.

2510KO2 - 10HP at 460V, 10HP at 600V
2510KO6 - 15HP at 460V, 20HP at 600V

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.