Browse FAQs

When installing an NQOD442L225CU, there is an arc flash warning label and another danger label that are upside down when the panel is inverted for top feed application. Will that pose a problem? Will it void the UL listing?

Published date: 11 June 2020

Issue:
Will the inverted Panel void the UL listing, for top feed application since the Warning Labels are upside down?

Product Line:
Panelboards

Environment:
NQOD

Cause:
Installation / Setup

Resolution:
No. Inverting the panel and having labels upside down is usually not an issue. It will not affect the panel rating. If there is a local code or inspection issue issue with this, it may be possible to obtain new arc flash and danger labels for the panel from your local Square D/Schneider Electric Distributor.


CTA-ID : 2037498

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.