{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
RXZL520 and RUZL420 Difference
Issue:
What is the difference between the RXZL520 and the RUZL420?

Product Line:
Relays and Timers

Environment:
RPM Plug-in Relay

Resolution:
The RXZL520 is a sheet of 108 clip on markers that mount to the front of the Zelio miniature R type relays relay in the bottom left hand corner. The RUZL420 are clip on markers (1 unit but sold in lots of 10) for the sockets with separate contacts for the RUM relay line.

Schneider Electric USA

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: