Browse FAQs

Is there an amber lens for ZB4 illuminated selector switches?

Published date: 21 June 2020

Issue:
Does the current ZB4 operator have amber lenses?

Product Line: 
Push Buttons and Operator Interface

Environment:
22mm Push Button 

Resolution:
There is not an amber offer, but you can use the yellow lens. It is almost the same color as the old amber unit.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.