Browse FAQs

Is the MCT12BC, listed in Digest 175 on page 15-6, available?

Published date: 12 June 2020

Issue:
is the part number MCT12BC available?

Product Line:
PTEQP - LV EQPT (IEC & NEMA)

Environment:
NFPA99, NEC517.160

Cause:
A change in how to order the clock/timer, with one part number or by using separate component part numbers, rendered the previously published catalog number invalid.

Resolution:

Note:  this product is obsolete and has been superseded by the Iso-Gard IGT Dual Clock/Timer.

Instead of MCT12BC, the device was ordered in component parts:  MCT12B, MCTS95135, 53007BB and MCTCT.
The system does not recognize MCT12BC but does recognize the four parts that make up this catalog number.


CTA-ID : 2040553

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.