Browse FAQs

Is there an support bracket available for a PTQ4680G fusible plug-in unit?

Published date: 17 June 2020

Issue:
Support bracket available for a PTQ4680G fusible plug-in unit

Product Line:
LV Busway

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. A new plug-in unit, however, will come with a support bracket. An ``H`` or a ``V`` at the end of the catalog number will indicate if the unit is design to mount on Horizontal or Vertical busway (i.e. PTQ4680GH or PTQ4680GV).

CTA-ID : 2043386

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.