Browse FAQs

Can you replace the Reset button on the 9065SP54 MotorLogic Plus overload?

Published date: 10 June 2020

Issue:
Is the reset button on the 9065SP54 MotorLogic Plus overload replaceable?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)

Resolution:
This button is not replaceable. The customer will have to replace the entire unit.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.