Browse FAQs

Is there an optional Main Lug Kit for the 600 ampere NQ panel?

Published date: 23 June 2020

Issue:
Does Square D offers optional Main Lug Kit for the 600 ampere NQ panel?

Product Line:
Panelboards.

Environment:
NQ Panelboards.

Cause:
Product Selection

Resolution:
Yes. AL Compression NQALV6, Copper Mechanical NQCUM6 and Copper Compression NQCUV6.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.