Browse FAQs

What does voltage code D49 for control power transformers indicate? Example 9070T100D49

Published date: 23 June 2020

Issue:
 Voltage Code D49 meaning for Control Power Transformers

Product Line:
Control Power Transformers

Environment:
Products sold and used in the United States

Cause:
Product Features

Resolution:
The D49 voltage code defines a 208/230/460/575 Primary input with a 120V Secondary output


CTA-ID : 2045951

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.