Browse FAQs

Looking for replacement parts of EE750T68H Transformer.

Published date: 24 June 2020

Issue:
What is the part number for the Enclosure Replacement parts for the EE750T68H transformer?

Product Line:
LV Transformer

Environment:
EE Transformer

Resolution:
Replacement parts for the 31D style Enclosure are:
Weathershield WS384

Enclosure Parts:

Top cover 4313505501
Front upper panel p/n is 4313505701(When replacing a front upper panel, specify the
transformer part number and with nameplate and labels on the order.)
Front lower panel p/n is 4313505801
Rear upper p/n is  4313505701
Rear lower p/n is 4313505801
Sides (ends) p/n is 4313505601
Base p/n is 4313506250
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.