Browse FAQs

What is the width of an NQ interior catalog number NQ442L4C?

Published date: 29 June 2020

Issue:
Width of an NQ interior NQ442L4C

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The width of the typical NQ interior from mounting hole to mounting hole is 10.44``. The rails are 11.5 inches from outside to outside. The DF is 12.3 inches wide.


CTA-ID : 2045396

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.