undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Are the mounting bolts used to mount the lugs in catalog number CMELK4 included with the kit?
Issue:
Lug mounting hardware

Product Line:
Metering Equipment

Resolution:
No, the mounting hardware or studs should already be installed on the lug landing pad of the metering device. This kit is supplied ONLY with (4) ILSCO lugs, catalog number TA6002N.

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: