Browse FAQs

Can the Main Contacts in a 8910DPA be converted to Normally Closed?

Published date: 29 June 2020

Issue:
Needs normally closed contacts using the 8910 definite purpose contactors

Product Line:
8910 Definite Purpose Contactors

Environment:
NEMA Contactors and Starters

Resolution:
Conversion of power contacts is not possible in the field nor can we provide a device with 3 normally closed poles.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.