Browse FAQs

Does Square D offer a 22k AIR rated QO-CAFI type breaker?

Published date: 14 May 2020

Issue:
Is there a 22k AIC rated QO-CAFI breaker?

Product Line:
QO Circuit Breakers

Environment:

QO-CAFI Circuit Breakers

Resolution:
Yes, 22kA Combination Arc-Fault breakers are available with a VH suffix.  For example, catalog numbers QO115VHCAFI and QO120VHCAFI carry a 22 kA interrupting rating at 240 Vac.  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.