{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a 8538SBG32 be converted to accept 30a 600v fuses ?
Issue:
Can the disconnect switch (9422FTCF30) used on 8538SBG32 series K combination starter be converted to accept 30a 600v fuses?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Disconnect switches

Resolution:
Yes, order a 9422TC33 conversion kit. Catalog Number RFK06 will also be needed if Class R fuse clips are required.

NOTE: Check the series of the combination starter

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.