Browse FAQs

What is the ATV71 and ATV61 Drive efficiency?

Published date: 02 June 2020

Issue:
 ATV71 and ATV61 Drive Efficiency.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to find what the ATV61 and ATV71 drives efficiency is.

Resolution:
Depending on HP size and voltage approx 98% at rated load.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.