Browse FAQs

What are the repair parts for a HU266R Series E2, E4 and E5 Heavy Duty Safety Switch?

Published date: 14 May 2020

Issue:
Repair Rarts for a HU266R Series E2, E4 and E5

Product Line:
Safety Switch

Environment:
Heavy Duty Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HUN226E2 (includes line base assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-186-50 SEL (2-required and arc suppressor assembly is not included)
Arc suppressor assembly - 40512-708-50 (2-required)
Lug assembly - 44050-446-01 (2 required per base assembly)
Line base phase insulator - 40552-193-01 (1 required)
Line base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Door thumb retainer - 44050-490-01
Door thumb screw - 44050-434-01
Cross Arm Insulator – (2) 40552-177-01 (left and right side pieces); (1) 40552-178-01 (center piece); (1) 40552-157-01 (dust shield – retainer for insulators)
Handle knob kit (black & red knob at end of handle) - Series E1 is 44011-427-50, Series E4 and E5 is 40283-435-50

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.