Browse FAQs

What is the part number for the handle and cable mechanism for MGL36600?

Published date: 14 May 2020

Issue:
Cable Operating Mechanism for MGL36600 

Product Line: 
Disconnect Switches 

Environment:
9422 Flexible Cable Mechanisms

Resolution:
It is 9422AP1 (sheet steel, NEMA 4) or 9422AP2 ( stainless NEMA 4, 4X) handle and 9422CMP40 for a 48 inch cable mechanism. There is also an option for 50 inch cable mechanism part number 9422CMP50 and the 120 inch 9422CMP10. See Digest 177 Section 8 page 8-41 to 8-42 tables 8.94 and 8.96.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.