Browse FAQs

What is the difference between the VW3A3315 and VW3A3319 BACnet option cards for the ATV61 drives?

Published date: 31 May 2018


Issue:
What is the difference between the VW3A3315 and VW3A3319 BACnet option cards for the ATV61 drives?

Product Line:
VW3A3315 and VW3A3319 

Environment:
All

Cause:
Wants to know what the differences are between the two cards. 

Resolution:
The BACnet option card for the Altivar 61 AC drive has been upgraded.
To facilitate this upgrade, the part number has changed from VW3A3315 to VW3A3319.
The old part number VW3A3315 will become obsolete.
The new BACnet option card (VW3A3319)  is equipped with a 4 position, removable connector in place of the female sub D 9 pin connector on the old option card.  
This change will make network connections easier, allow installers to daisy chain network wiring and reduce installation time.
The new VW3A3319 manual is ATV61_bacnet_EN_1765274_04  See the PDF file attachment to view new manual.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.