Browse FAQs

What is the difference between the 80114-098-52 and PK22FL?

Published date: 07 July 2020

Issue:
Difference between part number 80114-098-52 and the PK22FL panelboard lock.

Cause:
Included contents of 80114-098-52

Resolution:
The 80114-098-52 is an interplant part number for the lock ONLY that is included with a PK22FL.  The PK22FL also includes a couple of screws.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.