Browse FAQs

On the ATV21 and ATV212 Drives, what parameter determines the allowed motor rotation direction?

Published date: 03 May 2018

Issue:
On the ATV21 and ATV212 Drives, what parameter determines the allowed motor rotation direction?

Product Line:
Altivar ATV21, ATV212

Environment:
All serial numbers

Cause:
Customer said drive won't run forward or reverse on remote.

Resolution:
Parameter F311 is the motor rotation direction command.
F311 = 0 is FWD and REV operation is permitted
F311 = 1 is FWD operation only factory default)
F311 = 2 is REV operation only


CTA-ID : 2062099

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.