Browse FAQs

What breakers can be used in a QO2L30S load center?

Published date: 14 May 2020

ISSUE:
What breakers will fit in a QO2L30S?

PRODUCT LINE:
Load Centers

ENVIRONMENT:
QO Load Centers

RESOLUTION:
The QO2L30S will accept (1) double pole or (2) single pole QO breakers. It will not accept type QO-EPD, QO-GFI, QO-AFI, QOB, QOT tandem or QO tandem circuit breakers. This is a 2 space/2 circuit panel, accepting full size QO branch circuit breakers only. The 30 ampere panel rating should not be exceeded, or 25 ampere when aluminum feeder wire is used.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.