Browse FAQs

ATV61 with the DeviceNet card VW3A3309 troubleshooting assistance.

Published date: 19 June 2020

Issue:
ATV61 with the DeviceNet card VW3A3309 troubleshooting assistance.

Product Line:
Altivar ATV61

Environment:
All ATV61 with optional VW3A3309 DeviceNet option cards.

Cause:
Drive will not start using network commands with DeviceNet option card installed on the drive.

Resolution:
Check the reference and command channel, make sure it is set for communications card control.
The PLC (Logix 5000) could read data, but was not able to write. Verified that I/O Scanner was set up properly, but the scanner module was Idle.
Restarted scanner module. 
Now, we find out the CMD and LFRD are DINT (32 bit words).  The 1st 16 bits of the word are the CMD, and the 2nd 16 bits are for the LFRD speed reference.
Customer needs to write to the 32 bit word accordingly for start/stop and speed reference.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.